Overview: .NET Wrapper

Sink a dataset to a .NET object that has been created in a separate application, prior to using this operation. This sink object will be a .NET assembly library file (dll). Using the .NET object will allow for reuse and  interchangeability of code and datasets between different programmes.

The .NET object previously created will determine in what format the dataset is exported, and will determine how the dataset needs to be configured in order to be utilized by the .NET object.  

NOTE: CSense provides secure native blocks and operations for building analytics and solutions. The native capabilities provided by CSense can be extended by making use of this feature. When making use of this feature, please ensure that you have validated your extended functions to ensure that they perform as intended and do not introduce stability or security risks to your production system. Do not use scripts or components from untrusted sources.

Properties

Category:

Export

Performance risk:

High potential performance risk. The performance is influenced by the size of the text file being imported, which is determined by number of rows and/or the number of columns of the dataset.

Knowledge required:

Working knowledge of the .NET object

 

Effect on datasets

How many datasets are required to perform this operation?

One

Does it create a new dataset?

N/A

Can you reconfigure this operation?

Yes

Can you apply this operation to a locked dataset?

Yes

Does it modify the current dataset in any way?

No

Requirements

  • A dataset with at least one field of any type.

Results

  • A new file will be created with the selected fields from the dataset.


Related topics:

  

CSense 2023- Last updated: June 24,2025